earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-B, Edge Server, AS-P
Fonctionnalités : Ingénierie, Matériel
Version produit : 2023
16/12/2022

Connecting to an Enterprise Server or Enterprise Central

You connect to an Enterprise Server or Enterprise Central so that you can set the servers to reset mode.

Afficher plus
action_close

You can reset the administrator password on your EcoStruxure Building Operation servers if you, for example, have locked yourself out.

Your local Schneider Electric Buildings support team provides you with a temporary password for logging on to EcoStruxure BMS so that you can change your administrator password.

Pour plus d'informations, voir Password Reset Workflow .

Déclaration
    • To set an Enterprise Server or Enterprise Central to reset mode you must run Device Administrator as an administrator. Refer to Windows how to run a program as an administrator.

    • Device Administrator must run on the same computer as Enterprise Server or Enterprise Central.

To connect to an Enterprise Server or Enterprise Central
  1. In Device Administrator, click Servers and then click Add server .

  2. In the EBO server type list, select Enterprise Server or Enterprise Central.

  3. Enter something in the Password box. The server is added even with an incorrect password.

  4. Click OK .

  • Administrator Password Reset