Wire Sizes and Lengths for the Digital Inputs of the RP Controller Expansion Modules
This section provides recommendations on wire sizes and lengths for the digital inputs of the RP controller expansion modules.
表格: Wire Sizes and Lengths for the Digital Inputs of the RP Controller Expansion Modules
Maximum Total Cable Resistance
|
Typical Cable
|
50 ohm (2 x 25 ohm)
|
266 m (873 feet) long cable with an area of 0.2 mm
2
(24 AWG) at 50 °C (122 °F)
|
I/O Wiring
Wire Sizes and Lengths
RP Controller Expansion Module Digital Inputs
Wire Sizes and Lengths for the DALI Bus of the RP Controller Expansion DALI Light Modules