You use the SpaceLogic Sensor
Display
property tabs in WorkStation to view and configure the UI features of the various sensor models within your control application.
The Display
Basic
tab properties includes the same
General Information
you find on all EcoStruxure Building Operation objects. Beyond that, it also provides a
Setpoint
, a
Fan speed
, an
Occupancy override
, an
HVAC mode
, a
Heating cooling status
, and 4
Custom value text
fields. In addition, there are several properties that allow you to control the temperature display. For example, the
Temperature display mode
allows you to configure the temperature value displayed on the SpaceLogic Sensor display in its passive display state with the following settings:
Live Temperature
: Displays the space temperature measured by the SpaceLogic sensors internal temperature sensor
Temperature setpoint
: Displays the current setpoint temperature value
Custom temperature
: Displays the value of the Custom temperature property
The Custom temperature property then allows you to display any value in the temperature range, either by referencing another temperature source (for example, an external temperature sensor) or by setting it manually in the Custom temperature field (warm start retained only).
Advanced Tab
The Display
Advanced
property tab includes considerably more configuration information. For example, you turn on the
Allow menu page
property to display all submenus including the Functions menu and any of its submenus. Should you wish, you can enable the temperature setpoint feature by setting the Display object
Allow setpoint changes
property to
On
and configuring the
Setpoint high limit
and
Setpoint low limit
properties. If colored wall back lighting feedback is required for the room occupant, you can turn on the
Enable wall back lighting
property.
Obs!
Allow setpoint changes, Setpoint high limit, and Setpoint low limit are the types of properties you may wish to drive dynamically based on time of day. For example, using a schedule, you may only allow setpoint changes during the day and not at night. You may also only change the high and low limits for the setpoint based on whether you are in the heating or cooling season.
In addition, you can use the
Occupancy override icon
property and its
Command
and
State
options as follows:
Command
: When occupied, the house is empty. When clicked, the Command to vacate or unoccupy is sent.
When unoccupied, the house displays with a person inside. When clicked, the Command to occupy is sent.
State
: When the house displays with a person inside, it indicates the current state is occupied. When clicked, the State command to unoccupy is sent.
When unoccupied, the house is empty to indicate its current state. When clicked, the State command to occupy is sent.
Finally, you can enable lighting and blind control functions using the Display object
Allow light control
and
Allow blind control
properties. Within the light function, you can toggle on and off or set a percentage to control the intensity of the lights using the
Lighting mode
property. Similarly, you can you can toggle on and off or set a percentage to control the blind louver sub-function using the
Blind control mode
property.
Light and Blind Control Tab
For more granular control, you can use the Light and Blind Control tab to specify the 4 supported light groups, and the blind position and angle for the 12 supported blind groups in the SpaceLogic Sensor. You can also use the
Light forced disable
and
Blind forced disable
properties as an override or a forced disable.
Light and Blind Configuration Tab
In this tab, you can enter the
Default light group
or
Default blind group
value corresponding to the Light and Blind Control tab
Light 1-4 level
and
Blind 1-12 position
properties. For example, if you select Default light group or Default blind group equals 1, you direct the Remote Control to affect the Light 1 level and the Blind 1 angle and Blind 1 position properties.
Button and Scene Configuration Tab
The Display
Button and Scene Configuration
property tab allows you to select from the available functions or scenes to program the buttons on the SpaceLogic Sensor display models. You can also select the buttons you wish to display for configured scenes and triggers for each of the scene buttons.
Mer information finns i Configuring SpaceLogic Sensor Display Properties
.
Property Mapping
While the Display property tabs allow you to configure varied SpaceLogic Sensor models with different UI features, not all of the properties apply to each model. Be sure to consider this when configuring the application and binding it to your control programs. The table that follows shows the properties applicable to each unit.
Tabell: SpaceLogic Sensor and Display Object Property Mapping
Display property
|
Touchscreen Display
|
LCD Temperature Sensor
|
3-Button Cover
|
Setpoint
|
Yes
|
Yes
|
Yes
|
Fan speed
|
Yes
|
Yes
|
No
|
Occupancy override
|
Yes
|
Yes
|
Yes
|
HVAC mode
|
Yes
|
Yes
|
No
|
Selected scene
|
Yes
|
Yes
|
No
|
Light level
|
Yes
|
Yes
|
No
|
Blind position
|
Yes
|
Yes
|
No
|
Blind slat angle
|
Yes
|
Yes
|
No
|
Temperature display mode
|
Yes
|
Yes
|
No
|
Custom temperature
|
Yes
|
Yes
|
No
|
Heating cooling status
|
Yes
|
Yes
|
No
|
Show time
|
Yes
|
No
|
No
|
Time format
|
Yes
|
No
|
No
|
Show CO2
|
Yes
|
Yes
|
No
|
Show humidity
|
Yes
|
Yes
|
No
|
Temperature units
|
Yes
|
Yes
|
No
|
Allowed fan speeds
|
Yes
|
Yes
|
No
|
Enable wall back lighting
|
No
|
No
|
Yes
|
Lighting mode
|
Yes
|
Yes
|
No
|
Blind control mode
|
Yes
|
Yes
|
No
|
Blind angle mode
|
Yes
|
Yes
|
No
|
Allowed HVAC modes
|
Yes
|
Yes
|
No
|
Allow setpoint changes
|
Yes
|
Yes
|
Yes
|
Setpoint high limit
|
Yes
|
Yes
|
Yes
|
Setpoint low limit
|
Yes
|
Yes
|
Yes
|
Allow fan speed changes
|
Yes
|
Yes
|
No
|
Allow occupancy overrides
|
Yes
|
Yes
|
No
|
Allow HVAC mode changes
|
Yes
|
Yes
|
No
|
Allow menu pages
|
Yes
|
No
|
No
|
Allow sensors information pages
|
Yes
|
No
|
No
|
Allow device information page
|
Yes
|
No
|
No
|
Allow parent information page
|
Yes
|
No
|
No
|
Allow custom information page
|
Yes
|
No
|
No
|
Allow temperature unit changes
|
Yes
|
Yes
|
No
|
Allow light control
|
Yes
|
Yes
|
No
|
Allow blind control
|
Yes
|
Yes
|
No
|
Display backlight
|
Yes
|
No
|
No
|
Button (1-12) function
|
Yes
|
Yes
|
No
|
Scene button (1-8) button
|
Yes
|
Yes
|
No
|
Scene button (1-8) trigger
|
Yes
|
Yes
|
No
|
SpaceLogic Living Space Sensor / Eco mode
|
Yes
|
Yes
|
Yes
|