Inherited licenses are EcoStruxure Building Operation software licenses that are inherited from an Enterprise Server by the attached SmartX servers.
When an inherited license is activated for the Enterprise Server all attached Smart servers can use the feature. Inherited licenses are activated using License Administrator and the EcoStruxure Building Operation Software License mechanism and workflow.
For more information, see EcoStruxure Building Operation Software Licensing Overview .
Inherited licenses apply to the following features on an Enterprise Server:
SNMP Notification
Personal Dashboard
Change Control
TimescaleDB
MQTT
For example, you want to use SNMP on some of your SmartX servers that are attached to an Enterprise Server. When you activate the SNMP license on your Enterprise Server, all attached SmartX servers are allowed to use SNMP.
Note however that the features, except Change Control, can also be used on a stand-alone SmartX server. In this case the licenses must be activated using the Device Administrator.