earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: AS-B, Device Administrator, AS-P
Funkcje: Zarządzanie licencją
Wersja produktu: 2022
2021-12-17

Inherited Licenses

Inherited licenses are EcoStruxure Building Operation software licenses that are inherited from an Enterprise Server by the attached automation servers.

When an inherited license is activated for the Enterprise Server all attached automation servers can use the feature. Inherited licenses are activated using License Administrator and the EcoStruxure Building Operation Software License mechanism and workflow.

Więcej informacji zawiera EcoStruxure Building Operation Software Licensing Overview .

For example, you want to use SNMP on some of your automation servers that are attached to an Enterprise Server. When you activate the SNMP license on your Enterprise Server, all attached automation servers are allowed to use SNMP.

Some features can also be used on a stand-alone automation server. In this case the licenses must be activated using the Device Administrator.

Więcej informacji zawiera Software and Features that Require Licenses .

  • EcoStruxure Building Operation Software Licensing Installation and Location
  • Automation Server Licensing Overview
  • Software and Features that Require Licenses