Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 2024, 7.0
03/12/2024

Deleting the Display Name and the IP Address of a Server

You delete the display name of the server address and/or the IP address of a server from the list when you no longer need it.

Afficher plus
action_close

You log on to WorkStation or WebStation to securely access the EcoStruxure BMS features.

Log on to WorkStation

You log on to WorkStation with your current Windows credentials, as another Windows user, or as an EcoStruxure BMS user. Your system administrator decides which type of user you log on as. ​

To log on to WorkStation using an EcoStruxure BMS account, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

To log on to WorkStation using a Windows account, you need to know the EcoStruxure BMS server.

The account information for both the EcoStruxure BMS account and the Windows account is provided by the system administrator.

Déclaration

​​Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation. Pour plus d'informations, voir EcoStruxure Building Operation Software Licensing Installation and Location .

Remember me on this computer

For a faster log on in Workstation, use the Remember me feature to automatically fill in your user name, password, domain and server. Both BMS users and Windows users can use the Remember me feature.

Add a display name of the server address

When you log on to a new server, its IP address is added to the server list. You can add a display name of the server address to make it easier to find your server in the list.

Log on to WebStation

To log on to WebStation, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

The account information for your account is provided by the system administrator.

To delete the display name and the IP address of a server
  1. In the WorkStation window , on the server addresses drop-down list box, highlight the IP address of the server you want to delete the settings of.

  2. Click the Delete button

     
    action_zoom_plus_stroke
    .

  • Log on to WorkStation or WebStation
  • Building Operation WorkStation Window
  • Display Names and IP Addresses of Servers Drop-Down List Box
  • Logging on to WorkStation as an EcoStruxure Building Operation User
  • Logging on to WorkStation using your Windows user account
  • Logging on to WorkStation as another Windows User
  • Saving Log On Details
  • Adding a Display Name of the Server Address
  • Editing the Display Name of the Server Address
  • Importing a List of the Display Names and IP Addresses of Servers
  • Exporting the List of the Display Names and IP Addresses of Servers
  • Clearing the List of the Display Names and IP Addresses of Servers