earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 3.2, 3.3, 2022
15/10/2020

Exporting the List of the Display Names and IP Addresses of Servers

You export the list of the display names of server addresses and IP addresses of servers to share it with other users of WorkStation and help them organizing their own list of display names easier.

Afficher plus
action_close

You log on to WorkStation or WebStation to securely access the EcoStruxure Building Operation functions.

Log on to WorkStation

You log on to WorkStation with your current Windows credentials, as another Windows user, or as an EcoStruxure Building Operation user. Your system administrator decides which type of user you log on as. ​

To log on to WorkStation using an EcoStruxure Building Operation account, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

To log on to WorkStation using a Windows account, you need to know the EcoStruxure BMS server.

The account information for both the EcoStruxure Building Operation account and the Windows account is provided by the system administrator.

Déclaration

​​Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation. Pour plus d'informations, voir EcoStruxure Building Operation Software Licensing Installation and Location .

Remember me on this computer

For a faster log on in Workstation, use the Remember me feature to automatically fill in your user name, password, domain and server. Both Building Operation users and Windows users can use the Remember me feature.

Add a display name of the server address

When you log on to a new server, its IP address is added to the server list. You can add a display name of the server address to make it easier to find your server in the list.

Log on to WebStation

To log on to WebStation, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

The account information for your account is provided by the system administrator.

To export the list of the display names and IP addresses of servers
  1. In the WorkStation window , on the server addresses drop-down list box, click the Export button

     
    action_zoom_plus_stroke
    .

  2. In the Save as  dialog box, browse to the location where you want to save your file.

  3. Click Save .

  • Log on to WorkStation or WebStation
  • Building Operation WorkStation Window
  • Display Names and IP Addresses of Servers Drop-Down List Box
  • Connexion à WorkStation en tant qu'utilisateur EcoStruxure Building Operation
  • Connexion à WorkStation à l'aide de vos identifiants Windows
  • Connexion à WorkStation sous un autre nom utilisateur Windows
  • Enregistrement des informations de connexion
  • Adding a Display Name of the Server Address
  • Editing the Display Name of the Server Address
  • Deleting the Display Name and the IP Address of a Server
  • Importing a List of the Display Names and IP Addresses of Servers
  • Clearing the List of the Display Names and IP Addresses of Servers