earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: RP-C
Functionalities: Hardware
Product version: 2022, 2023, 2024, 7.0
3/11/2022

Zigbee Modules Reset Button

The RP controller expansion Zigbee modules have a Reset button on the front.

 
action_zoom_plus_stroke Zigbee Modules Reset Button (Example for RP-C-EXT-ZB-DALI)
Figure: Zigbee Modules Reset Button (Example for RP-C-EXT-ZB-DALI)

You can reset the Zigbee modules depending on how long you press the reset button.

Table: Reset Modes

Mode

Description

Factory reset

Press and hold the Reset button for 5 seconds.

The device is reset to factory settings.

During the reset process, the LED shows fast flashing red light. When the reset is completed, the LED returns to constant green light. For more information, see Zigbee Modules LED .

  • RP Controller Expansion Zigbee Modules
  • RP-C-EXT-ZB-DALI
  • RP-C-EXT-ZB-0-10V
  • Zigbee Modules LED