The RP controller expansion Zigbee modules have fixed screw terminals for the power input, power output, and light output.
The wiring recommendations are provided separately. For more information, see Wiring .
The Zigbee DALI module is equipped with eight fixed screw terminals.
For more information, see Zigbee DALI Module Screw Terminals .
The Zigbee 0-10V module is equipped with eight fixed screw terminals.
For more information, see Zigbee 0-10V Module Screw Terminals .