earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: User Management
Product version: 2023, 2024
12/16/2022

Unify Domains in the Server Structure Workflow

Use this workflow to unify domains and to make sure all the servers have the same domain after you add an Enterprise Central to your system. Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Unify domains in the server structure workflow
Figure: Unify domains in the server structure workflow
Log On to the Enterprise Server

Log on to the Enterprise Server that you want to add to the Enterprise Central. For more information, see Log on to WorkStation or WebStation .

Export the Domain

Export the domain you want to use from the Enterprise Server. For more information, see Import and Export of User Management Solutions .

Delete the Domain

Delete the domain from the Enterprise Server to avoid conflict. For more information, see Deleting a Domain .

Log On to the Enterprise Central

Log on to your Enterprise Central in order to import your domain and add the servers. For more information, see Log on to WorkStation or WebStation .

Import the Domain

Import the domain that you want to use to the Enterprise Central. For more information, see Import and Export of User Management Solutions .

Add the Enterprise Server

Add the Enterprise Server to the Enterprise Central. For more information, see Adding an Existing Enterprise Server to an Enterprise Central .

Add the Enterprise Server to your domain

Add the Enterprise Server to the domain of the Enterprise Central. For more information, see Adding an Existing Enterprise Server to an Enterprise Central .

Add your Automation Servers to the domain

Add your automation servers to the domain of the Enterprise Server. For more information, see Assigning an Automation Server to a Domain .

  • Domains
  • Multi-server Systems
  • Enterprise Central
  • Automation Servers
  • Log on to WorkStation or WebStation
  • Import and Export of User Management Solutions
  • Deleting a Domain
  • Adding an Existing Enterprise Server to an Enterprise Central