earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 用户管理
产品版本: 2.0, 2.1, 3.0, 3.1
2020/8/18

Unify Domains in the Server Structure Workflow

Use this workflow to unify domains and to make sure all the servers have the same domain after you add an Enterprise Central to your system. Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Unify domains in the server structure workflow
图: Unify domains in the server structure workflow
Log On to the Enterprise Server

Log on to the Enterprise Server that you want to add to the Enterprise Central. 有关更多信息,请参阅 登录 WorkStation 或 WebStation .

Export the Domain

Export the domain you want to use from the Enterprise Server. 有关更多信息,请参阅 Import and Export of User Management Solutions .

Delete the Domain

Delete the domain from the Enterprise Server to avoid conflict. 有关更多信息,请参阅 Deleting a Domain .

Log On to the Enterprise Central

Log on to your Enterprise Central in order to import your domain and add the servers. 有关更多信息,请参阅 登录 WorkStation 或 WebStation .

Import the Domain

Import the domain that you want to use to the Enterprise Central. 有关更多信息,请参阅 Import and Export of User Management Solutions .

Add the Enterprise Server

Add the Enterprise Server to the Enterprise Central. 有关更多信息,请参阅 Adding an Existing Enterprise Server to an Enterprise Central .

Add the Enterprise Server to your domain

Add the Enterprise Server to the domain of the Enterprise Central. 有关更多信息,请参阅 Adding an Existing Enterprise Server to an Enterprise Central .

Add your SmartX Servers to the domain

Add your SmartX Servers to the domain of the Enterprise Server. 有关更多信息,请参阅 Assigning a SmartX Server to a Domain .

  • Domains
  • Multi-server Systems
  • Enterprise Central
  • SmartX Servers
  • 登录 WorkStation 或 WebStation
  • Import and Export of User Management Solutions
  • Deleting a Domain
  • Adding an Existing Enterprise Server to an Enterprise Central