earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 2023, 2024
12/16/2022

Mass Copying Selected Properties

You mass-copy selected properties from an object configuration to other objects of the same type, in order to re-use the configuration.

The dialog Copy selected properties from … only display writeable properties visible in the property grid. Properties on sub objects are not displayed in the dialog.

Show More
action_close

Use mass edit when you want to change several property values or rename several objects at a time.

You can change several property values at a time, for example, when you want to change all setpoints from 22 to 20. For more information, see Mass Editing Objects .

 
action_zoom_plus_stroke Multi editing
Figure: Multi editing

The objects do not need to be of the same type to be mass edited. However, the properties you want to edit have to be of the same type.

You can mass rename all objects that are possible to move. For example, you can rename alarms but not properties.

You can rename the objects one by one. You can also copy row-separated text from a file, such as an MS Excel file, and paste it to rename several rows in one single operation. When you paste, the copied text is pasted from the row you have clicked and down in the list. If the copied text is longer than the number of rows, pasting stops at the last row.

For more information, see Mass Renaming Objects  .

For more information, see Mass Renaming Objects Using Copy and Paste  .

When you hover over the names in the Name column, the full path of the object is displayed.

You can mass change the units of objects in a search result. For more information, see Mass Changing Units .

To mass copy selected properties
  1. In the List View , select the objects you want to copy the properties to.

  2. On the Actions menu, point to Advanced and then click Copy properties from…

  3. In the Copy Properties From dialog box, select the object you want to copy properties from.

  4. Click Select .

  5. In the [Object] dialog box, select the properties you want to copy.

  6. Click OK .

The selected properties are now copied to all the selected objects.

  • Mass Edit
  • Actions Menu
  • Actions Menu – Advanced Submenu
  • Mass Editing Objects