earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 3.0, 3.1
2019/12/16

Checking the Integrity of an Alarm

You check the integrity of an alarm to verify that the path is valid.

显示更多
action_close

When an alarm is triggered it appears in the alarm list. You can acknowledge, disable, or hide alarms in the alarm list. An acknowledged alarm disappears from the alarm list when it has been reset to normal state.

When the alarm database gets corrupted after an EcoStruxure BMS server crash, all alarms are re-evaluated. The alarms that are still active are resent to the alarm database. However, the information that an alarm has been acknowledged, disabled, or hidden is lost, and you have to repeat operations you performed on the alarm before the data loss.

When an alarm has been triggered and reset to normal state without having been acknowledged, the alarm remains in the alarm list until it is acknowledged. If the alarm is lost, an alarm refresh does not make the alarm reappear in the alarm list. The alarm is reset and has no alarm state to send.

Most system information alarms are only messages. These alarms cannot be in an alarm state, thus, an alarm refresh does not make the system information alarms reappear in the alarm list.

To check the integrity of an alarm
  1. In Workstation log on to the server that has the alarms you want to check.

    重要:

    You start with the server that is the lowest in the hierarchy.

  2. In the System Tree pane, select System , and then select Alarm Control Panel.

  3. In the Actions menu, click Advanced , and then click Alarms integrity check .

  • Alarm Handling Issues
  • Alarm Cannot be Acknowledged Due to Invalid Paths