You install an RP controller expansion Zigbee module on a ceiling to properly fasten the device.
The RP controller expansion Zigbee modules are designed to be installed on a flat surface on a ceiling.
The Zigbee modules must be professionally installed to comply with the following rules and regulations:
2014/53/EU Radio Equipment Directive (RED) of the European Union (EU)
UK Statutory Instruments 2017 No. 1206 – The Radio Equipment Regulations 2017
有关更多信息,请参阅 Zigbee Modules Regulatory Compliance and Approvals .
The Zigbee module and its integrated antenna must be installed to provide a separation distance of at least 20 cm (8 in.) from all persons and must not be co-located or operating in conjunction with any other antenna or transmitter. Information on recommended RF exposure limits can be obtained from Health Canada's website, www.canada.ca/en/health-canada .
![]() |
---|
RADIO FREQUENCY (RF) EXPOSURE
Failure to follow these instructions can result in minor or moderate injury. |
通知 |
---|
REDUCED RADIO COVERAGE RANGE Do not route power or high-voltage cables close to the Zigbee module's integrated antenna, which is in the lower right area of the device. Failure to follow these instructions can result in reduced device performance. |
To install a Zigbee module on a ceiling, you drill two holes in the ceiling with a distance of 121 mm (4.7 inches) between the holes, and fasten the device using two M3 (3 mm) x 22 mm Phillips flat head self-tapping screws with a 5.8 mm screw head diameter. The device has two holes in the back cover to facilitate installation. The two screws are delivered with the device. 有关更多信息,请参阅 Installing an RP Controller Expansion Zigbee Module on a Ceiling .
The screw terminals on the left and right side of the Zigbee module are covered by two terminal covers (doors), which are intended to reduce the access to the screw terminals and wires. To open or close a terminal cover, you need to unscrew or screw in the two clamping screws. These two screws are also used to fasten the cables to the device. The device is equipped with an upper cable clamping bar on the inside of the terminal covers, and four lower cable clamping bars are delivered with the device, to facilitate the fastening of the cables. The lower, removable cable clamping bars can be mounted or removed to fit cables of smaller or larger diameter. 有关更多信息,请参阅 Wiring a Screw Terminal on an RP Controller Expansion Zigbee Module .
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH Disconnect the power supply and other high voltage equipment before wiring. Failure to follow these instructions will result in death or serious injury. |
![]() |
---|
RADIO FREQUENCY (RF) EXPOSURE
Failure to follow these instructions can result in minor or moderate injury. |
通知 |
---|
REDUCED RADIO COVERAGE RANGE Do not route power or high-voltage cables close to the Zigbee module's integrated antenna, which is in the lower right area of the device. Failure to follow these instructions can result in reduced device performance. |
Refer to the dimensional drawings before installing the Zigbee module.
Ensure that you have the proper mounting hardware and anchoring system.
Check the weight-bearing load before choosing your mounting hardware.
Find a suitable location and surface on which to mount the Zigbee module.
Loosen the screws that hold the two green terminal covers (doors) in place and then open the doors.
Hold the device in place against the ceiling.
Level the device.
Mark the place where the two drill holes (for attachment of the device) should be on the ceiling.
The distance between the two holes is 121 mm (4.7 inches).
Remove the device.
Drill two holes that fit M3 (3 mm) x 22 mm screws (or anchoring system per manufacturing specification).
Put the device in place on the ceiling and fasten the device using the two screws delivered with the device.
The device is delivered with two M3 (3 mm) x 22 mm Phillips flat head self-tapping screws with a 5.8 mm screw head diameter.
You can now wire the Zigbee module.