earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Tendencias
Versión del producto: 3.2, 3.3, 2022
15/10/2020

Create Object Wizard - Configure Log Processing Trend Log

Use the Configure Log Processing Trend Log of the Create Object wizard to create a log processing trend log to enable calculation within or between various trend logs.

 
action_zoom_plus_stroke Log Processing Trend Log dialog box
Figura: Log Processing Trend Log dialog box

Tabla: Log Processing Trend Log

Component

Description

Start time

Enter the starting date and time of the calculation.

Period interval

Type the time span of the calculation.

Trend logs

Displays trend logs that are used in the calculation.

 
action_zoom_plus_stroke

Click to add a trend log to be used in the calculation.

 
action_zoom_plus_stroke

Click to edit a trend log that is used in the calculation.

 
action_zoom_plus_stroke

Click to delete a trend log from the calculation.

Name

Displays the name of the trend log.

Calculation type

Displays the type of the calculation.

Use last known value

Displays the last known value of the calculation.

Calculation value

Type the formula for the calculation. Para obtener más información, consulte Log Processing Trend Log .

Quick filter

Displays the list of available log processing trend logs.

Time zone

Select the time zone for your calculations.

Displaying timestamp

Select the point in calculations where you want your timestamp to be inserted.

Unit

Enter the unit of your log.

Last logged value

Displays the last logged value.

Last logged timestamp

Displays the date and time of the last logged timestamp

Fetch delay (min)

Select the waiting time before the calculation starts.

Persist data

Select True to store data in the database.

  • Log Processing Trend Log
  • Creating a Log Processing Trend Log