earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Tendências
Versão do produto: 3.2, 3.3, 2022
15-10-2020

Configure Log Processing Trend Log Item Dialog Box

Use the Configure Log Processing Trend Log Item dialog box of the Create Object wizard to create a log processing trend log to enable calculation within or between various trend logs.

 
action_zoom_plus_stroke Configure Log Processing Trend Log dialog box
Imagem: Configure Log Processing Trend Log dialog box

Tabela: Configure Log Processing Trend Log Dialog Box

Component

Description

Log reference

Enter the unique identifier of your trend log.

Name

Type the name of your trend log.

Calculation type

Select the calculation type for your trend log.

Use last known value

Select True to use the last know value from the trend log.

Log unit

Enter the input unit of your log.

Target unit

Enter the output unit of your log.

Log guid

Displays the unique identifier of the log.

  • Log Processing Trend Log
  • Configuring Log Processing Trend Log