The remote control (RP-C-RC-BLE) is delivered with a base that allows the remote control to be installed on a wall or partition.
The remote control must be professionally installed and serviced to comply with the following rules and regulations:
Part 15 of the Federal Communications Commission (FCC) rules
Innovation, Science and Economic Development Canada (ISED) licence-exempt Radio Standards Specifications (RSSs)
2014/53/EU Radio Equipment Directive (RED) of the European Union (EU)
S.I. 2017/1206 - Radio Equipment Regulations 2017 of the United Kingdom (UK)
Более подробную информацию см. Remote Control Regulatory Compliance and Approvals .
The base supports the following alternative installation methods:
Installation on a wall using adhesive tape
Installation on a wall using two self-tapping screws with flat countersunk screw heads
For example, you can use two Philips 4.2 mm (0.165 in.) diameter self-tapping screws with flat countersunk screw head of diameter 8.1 mm (0.319 in.).
The remote control can be fixed in the base. For example, you can use a Philips 2.2 mm (0.087 in.) diameter self-tapping machine screw with a 4.3 mm (0.169 in.) diameter flat countersunk screw head and a maximum length of 13 mm (0.512 in.).