This section provides recommendations on wire sizes and lengths for the DALI bus of the Zigbee DALI module (RP-C-EXT-ZB-DALI).
The DALI bus is connected to the Light outputs of the Zigbee DALI module. The Light outputs have two terminals, labeled DA+ and DA-, to which the two-wire bus is connected.
The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.
Only copper wires should be used for the DALI bus.
Minimum Cross-sectional Area | Cable Length |
0.75 mm² (18 AWG) | Up to 150 m (492 ft) |
1.0 mm² (17 AWG) | Up to 200 m (656 ft) |
1.5 mm² (15 AWG) | Up to 300 m (984 ft) |