earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: RP-C
Функции: Аппаратное обеспечение
Версия продукта: 2022, 2023, 2024, 7.0
11.03.2022

Wire Sizes and Lengths for the DALI Bus of the Zigbee DALI Module

This section provides recommendations on wire sizes and lengths for the DALI bus of the Zigbee DALI module (RP-C-EXT-ZB-DALI).

The DALI bus is connected to the Light outputs of the Zigbee DALI module. The Light outputs have two terminals, labeled DA+ and DA-, to which the two-wire bus is connected.

The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.

Only copper wires should be used for the DALI bus.

Таблица: Wire Sizes and Lengths for the DALI Bus of the Zigbee DALI Module

Minimum Cross-sectional Area

Cable Length

0.75 mm² (18 AWG)

Up to 150 m (492 ft)

1.0 mm² (17 AWG)

Up to 200 m (656 ft)

1.5 mm² (15 AWG)

Up to 300 m (984 ft)

  • I/O Wiring
  • Wire Sizes and Lengths
  • Wire Sizes and Lengths for the RP Controller Expansion Zigbee Modules
  • Zigbee DALI Light Output and Power Output