earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2023
2022/12/17

Users Substitution Codes

Users substitution codes represent the information you want to display when a notification report is triggered. The information is dynamically filled in from the users that are included in the notification report.

表格: Users Substitution Codes for Notification Reports

Code

Description

@(ActiveCommandPermissions)

Writes the active command permissions of the user.

@(ActiveGroupPolicies)

Writes the active group policies of the user.

@(ActivePathPermissions)

Writes the active path permissions of the user.

@(ActiveTypePermissions)

Writes the active type permissions of the user.

@(Description)

Writes the description.

@(DomainName)

Writes the domain a user belonged to.

@(ExpiryDate)

Writes the expiration date.

@(FirstName)

Writes the first name of the user.

@(HomeEmailAddress)

Writes the home email address of the user.

@(LastName)

Writes the last name of the user.

@(MemberOf)

Writes the names of groups the user belongs to.

@(MiddleName)

Writes the middle name of the user.

@(Note1)

Writes an event note.

@(Note2)

Writes another event note.

@(PathPermissions)

Writes the path permissions for the user.

@(ServerName)

Writes the server name.

@(TypePermissions)

Writes the type permissions for the user.

@(UserName)

Writes the user name of the user that generated the event.

@(WorkEmailAddress)

Writes the work email address.

@(Workspaces)

Writes the workspaces the user can access.

  • Notification Reports
  • Alarms Substitution Codes
  • Events Substitution Codes
  • Groups Substitution Codes
  • Multi Log List Substitution Codes
  • Properties and Watch View Properties Substitution Codes
  • Trend Log Records Substitution Codes