earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2024, 7.0
12/3/2024

Create Report Data Wizard - Configure Alarms Page

Use the Configure Alarms page to configure the content and the presentation of data in a notification report template.

 
action_zoom_plus_stroke Configure Alarms page
Figure: Configure Alarms page

Table: Configure Alarms Page

Component

Description

Name

Type a name for the data type group.

Add relative source

Select to enable adding a relative source to the filter.

Relative to

Enter the object with the relation to the notification report template that you want to use as a template for where notification reports are generated.

Relative source

Enter the object in relation to the Relative to property.

S ource preview

View how the source appears in the notification report text.

 
action_zoom_plus_stroke

Add

Click to add events to the notification report template.

 
action_zoom_plus_stroke

Remove

Click to remove the selected event from the notification report template.

 
action_zoom_plus_stroke

Clear all

Click to remove all events from the notification report template.

Template

Enter the text or substitution codes you want to use in the notification report.

Quick filter

Enter a word to filter on. For more information, see Quick Filter ..

Substitution codes list

Add the substitution codes you want to use in the notification or notification report.

Template delimiter

Enter the delimiter you want to use to separate the alarm records, event records, groups, search result, trend records, users or Watch View properties in the notification report.

Preview

View how the alarms, events, groups, properties, multi log list, trend log records, users, watch and also search results appear in the notification report text.

Substitute missing data with

Enter the text that is displayed when a value is missing. By default, a missing value displays nothing at all.

Number of alarms

Enter the maximum number of alarm records to add to the notification report.

Time range

Enter the time range for alarms included in the notification report.

Custom time range

Enter the number of days, hours and minutes that are to be included in the notification report.

  • Notification Reports
  • Alarms Substitution Codes
  • Quick Filter
  • Create Report Data Wizard - Configure Events Page
  • Create Report Data Wizard - Configure Groups Page
  • Create Report Data Wizard - Configure Multi Log List Page
  • Create Report Data Wizard - Configure Properties Page
  • Create Report Data Wizard - Configure Relative Properties Page
  • Create Report Data Wizard – Configure Relative Search Page
  • Create Report Data Wizard - Configure Relative Trend Log Page
  • Create Report Data Wizard – Configure Relative Watch View Page
  • Create Report Data Wizard – Configure Search Page
  • Create Report Data Wizard - Configure Trend Log Page
  • Create Report Data Wizard - Configure Users Page
  • Create Report Data Wizard – Configure Watch Page