earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2024, 7.0
2024/12/3

Create Report Data Wizard - Configure Users Page

Use the Configure Users page to configure the content and the presentation of data in a notification report template.

 
action_zoom_plus_stroke Configure Users page
图: Configure Users page

表格: Configure Users Page

Component

Description

Name

Type a name for the data type group.

Template

Enter the text or substitution codes you want to use in the notification report.

Quick filter

Enter a word to filter on. 有关更多信息,请参阅 Quick Filter ..

Substitution codes list

Add the substitution codes you want to use in the notification or notification report.

Template delimiter

Enter the delimiter you want to use to separate the alarm records, event records, groups, search result, trend records, users or Watch View properties in the notification report.

Preview

View how the alarms, events, groups, properties, multi log list, trend log records, users, watch and also search results appear in the notification report text.

Substitute missing data with

Enter the text that is displayed when a value is missing. By default, a missing value displays nothing at all.

Permission template

Enter the permission templates.

Type permission template

Enter the type permissions template.

Audit trial template

Enter the text or substitution codes you want to use in the notification report.

Quick filter

Enter a word to filter on. 有关更多信息,请参阅 Quick Filter ..

Substitution codes list

Add the substitution codes you want to use in the notification or notification report.

Number of events

Enter the maximum number of event records to add to the notification report.

Time range

Enter the time range for users included in the notification report..

Custom time range

Enter the number of days, hours and minutes that are to be included in the notification report.

Include related events

Select to include users with the same Operation ID used in Change Control. 有关更多信息,请参阅 Change Control .

Audit trial filter Settings

Configure conditions to the notification reports.

 
action_zoom_plus_stroke

Add

Click to add conditions to the notification report template.

 
action_zoom_plus_stroke

Remove

Click to remove the selected conditions from the notification report template.

 
action_zoom_plus_stroke

Clear all

Click to remove all conditions from the notification report template.

  • Notification Reports
  • Users Substitution Codes
  • Quick Filter
  • Change Control
  • Create Report Data Wizard - Configure Alarms Page
  • Create Report Data Wizard - Configure Events Page
  • Create Report Data Wizard - Configure Groups Page
  • Create Report Data Wizard - Configure Multi Log List Page
  • Create Report Data Wizard - Configure Properties Page
  • Create Report Data Wizard - Configure Relative Properties Page
  • Create Report Data Wizard – Configure Relative Search Page
  • Create Report Data Wizard - Configure Relative Trend Log Page
  • Create Report Data Wizard – Configure Relative Watch View Page
  • Create Report Data Wizard – Configure Search Page
  • Create Report Data Wizard - Configure Trend Log Page
  • Create Report Data Wizard – Configure Watch Page