earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concetto

Concetto


Prodotti: RP-C, RP-C-EXT-KNX
Funzionalità: Hardware
Versione del prodotto: 3.2, 3.3, 2022, 2023, 2024, 7.0, 7.1
01/09/2020

KNX Modbus Gateway Programming Mode

When the KNX Modbus gateway (RP-C-EXT-KNX) is in programming mode, you can assign an individual address to the device on the KNX bus.

You put the KNX Modbus gateway in programming mode by either pressing the Programming button or pressing the KNX write and KNX read buttons at the same time. Per maggior informazioni, consulta KNX Modbus Gateway Buttons .

When the device is in programming mode, the Programming LED and Mode LED are lit red. Per maggior informazioni, consulta KNX Modbus Gateway LEDs .

If required, the KNX Modbus gateway can be reset to factory default settings. Per maggior informazioni, consulta Performing a Factory Reset of the KNX Modbus Gateway .

  • Hardware Overview
  • KNX Modbus Gateway RP-C-EXT-KNX
  • KNX Modbus Gateway Buttons
  • KNX Modbus Gateway LEDs
  • Performing a Factory Reset of the KNX Modbus Gateway