When the KNX Modbus gateway (RP-C-EXT-KNX) is in programming mode, you can assign an individual address to the device on the KNX bus.
You put the KNX Modbus gateway in programming mode by either pressing the Programming button or pressing the KNX write and KNX read buttons at the same time. Более подробную информацию см. KNX Modbus Gateway Buttons .
When the device is in programming mode, the Programming LED and Mode LED are lit red. Более подробную информацию см. KNX Modbus Gateway LEDs .
If required, the KNX Modbus gateway can be reset to factory default settings. Более подробную информацию см. Performing a Factory Reset of the KNX Modbus Gateway .