earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: RP-C, RP-C-EXT-KNX
功能: 硬件
产品版本: 3.2, 3.3, 2022, 2023, 2024, 7.0
2020/9/1

KNX Modbus Gateway Programming Mode

When the KNX Modbus gateway (RP-C-EXT-KNX) is in programming mode, you can assign an individual address to the device on the KNX bus.

You put the KNX Modbus gateway in programming mode by either pressing the Programming button or pressing the KNX write and KNX read buttons at the same time. 有关更多信息,请参阅 KNX Modbus Gateway Buttons .

When the device is in programming mode, the Programming LED and Mode LED are lit red. 有关更多信息,请参阅 KNX Modbus Gateway LEDs .

If required, the KNX Modbus gateway can be reset to factory default settings. 有关更多信息,请参阅 Performing a Factory Reset of the KNX Modbus Gateway .

  • Hardware Overview
  • KNX Modbus Gateway RP-C-EXT-KNX
  • KNX Modbus Gateway Buttons
  • KNX Modbus Gateway LEDs
  • Performing a Factory Reset of the KNX Modbus Gateway