A backup of the semantic database is done automatically every time you do a backup of the Enterprise server.
The Semantic backup files are not part of the Enterprise server backup files (.xbk). The Semantic backup files are files on their own, but they are located in the same folder as the Enterprise server backup files.
If you make a Windows backup of you EBO system, do not forget to back up your Semantic backup files.
The semantic backup files are located in C:\ProgramData\Schneider Electric EcoStruxure\Building Operation X.X\Enterprise Server\db_backup\LocalBackup
The semantic database backup files are named <server><date>.trig.
You can restore a semantic database using the semantic backup file.
When you restore an Enterprise server you automatically restore the semantic database using the latest semantic database backup file.
For more information, see Restoring a Semantic Database .