You create a log processing trend log to enable calculation within or between various trend logs.
In Workstation, in the System Tree pane select the folder where you want to create the log processing trend log.
On the File menu, point to New, and then click Trend .
In the object type list, select Log Processing Trend Log .
In the Configure Log Processing Trend Log dialog box of the Create Object wizard, in the Name box, type the name of your log.
In the Path , select the folder where you want to create the log processing trend log .
In the Description box, type a description for the trend log.
Click Next .
In the Start time boxes, enter the starting date and the starting time of the calculation.
In the Period interval box, type the time span of the calculation.
Click
In the Choosing the Type and Naming the Object dialog box of the Create Object wizard, Name box, type the name of your trend log.
In the Path box, select the folder where you want to create the log processing trend logs.
In the Description box, type a description for the trend log.
Click Next .
In the Configure Log Processing Trend Log Item dialog box of the Create Object wizard, in the Log reference box, select the unique identifier of your trend log.
In the Name box, type the name of your trend log.
In the Calculation type box, select the calculation type for your trend log.
In the Use last know value , select True to use the last know value from the trend log.
In the Log unit , enter the input unit of your log.
In the Target unit , enter the output unit of your log.
In the Log guid , select the unique identifier of the log.
Click Create .
In the Configure Log Processing Trend Log dialog box of the Create Object wizard, select a trend log from the filter that you added and that are displayed in the Quick filter list.
In the Time zone box, select the time zone for your calculation.
In the Displaying timestamp select the point in calculations where you want your timestamp to be inserted.
In the Unit , enter the unit of your log.
In the Fetch delay , select the waiting time before the calculation starts.
In the Persist data , select True to store data in the database.
Storing the data in a database can increase performance if you have multiple Log Processing Trend Logs.
Click Create .