Produkty: RP-C-RC-BLE
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 3.2, 3.3, 2022, 2023, 2024, 7.0
2020-11-10

Temperature Screen

Use the Temperature screen to change the temperature setpoint.

 
action_zoom_plus_stroke Temperature screen
Rysunek: Temperature screen

Tabela: Temperature Screen

Component

Description

Temperature

Displays the temperature setpoint.

(room name)

Displays the name of the room or location.

 
action_zoom_plus_stroke

Press the - key to decrease the temperature setpoint with 0.5° for each press.

 
action_zoom_plus_stroke

Press the + key to increase the temperature setpoint with 0.5° for each press.

 
action_zoom_plus_stroke

Press the left context-sensitive key to go to the Home screen.

  • Remote Control Overview
  • Home Screen