earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WebStation
Funkcje: Trendy
Wersja produktu: 3.2, 3.3, 2022, 2023
2020-07-15

Creating a Trend Log List in WebStation

You create a trend log list to display values from a trend log in a list.

Pokaż więcej
action_close

A trend log list displays all values in the trend log in a list.

In the trend log list, you can perform the following tasks:

  • View all the values and their time stamp.

  • Add and edit records, for example if you knew that some records might be wrong or are missing.

  • Export values as an Excel file.

  • Export values as an xml file.

  • View meter log changes.

  • View events.

  • Change the settings.

 
action_zoom_plus_stroke A Trend log list in WebStation
Rysunek: A Trend log list in WebStation

To create a trend log list in WebStation
  1. In WebStation, right-click the trend log.

  2. Click Create trend item and then click Trend list .

  3. Click Save .

  4. In the Save - Trend Log List dialog box, in the Enter a new name box, type the name.

  5. In the Path box, enter the location.

  6. Click OK .

  • Trend Log Lists in WebStation
  • Trend Log List View
  • Trend Log List Toolbar in WebStation
  • Opening a Trend Log List
  • Meter Function
  • Managing Meter Replacement