earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2024, 7.0
2024/12/2

Property Context Menu – New Submenu

Use the New submenu to create new objects.

 
action_zoom_plus_stroke Property context menu - New submenu
图: Property context menu - New submenu

表格: Property Context Menu - New Submenu

Command

Description

Alarm

Click to open the Create Object wizard where you create an alarm. 有关更多信息,请参阅 Create Object Dialog – Naming the Object Page .

An alarm monitors a variable and alerts you if the monitored variable matches the configured alarm conditions. 有关更多信息,请参阅 Alarms Overview .

Trend

Click to open the Create Object wizard where you create trend logs, trend log lists, or trend charts. 有关更多信息,请参阅 Create Object Dialog – Naming the Object Page .

The function of a trend log is to log the variable that it is connected to and store the records. 有关更多信息,请参阅 Trends Overview .

  • Property Context Menu
  • Property Context Menu