Produkty: WebStation
Funkcje: Dashboards
Wersja produktu: 2022, 2023
2024-02-23

Dashboard Toolbar

Use the Dashboard toolbar to configure the dashboard and resize, clone, rebind and remove widgets from a dashboard.

Tabela: Dashboard Toolbar

Button

Description

 
action_zoom_plus_stroke

Save

Click to save changes in a dashboard.

 
action_zoom_plus_stroke

Add

Click to open the Select dashboard widget dialog box to add widgets to the dashboard.

 
action_zoom_plus_stroke

Settings

Click to open the properties dialog box for the dashboard.

 
action_zoom_plus_stroke

Select item s

Click to open the Dashboard toolbar to select, deselect, clone, remove or rebind a widget.

 
action_zoom_plus_stroke

Select all

Click to select all widgets in in the dashboard.

 
action_zoom_plus_stroke

Deselect all

Click to deselect alla widgets in the dashboard.

 
action_zoom_plus_stroke

Clone selected item

Click to clone the selected widget(s).

 
action_zoom_plus_stroke

Remove selected item(s)

Click to remove the selected widget(s).

 
action_zoom_plus_stroke

Rebind widget reference

Click to rebind a widget reference.

  • Dashboard Widgets
  • Configuring a Dashboard
  • Rebinding Widgets References
  • Cloning a Dashboard Widget