earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: WebStation
Функции: Dashboards
Версия продукта: 2024, 7.0
03.12.2024

Event Pareto Chart Dialog Box

Use the Event Pareto Chart dialog box to configure and edit an event Pareto chart.

 
action_zoom_plus_stroke Event Pareto Chart dialog box
Рисунок: Event Pareto Chart dialog box

Таблица: Event Pareto Chart Dialog Box

Component

Description

Column

Select the column(s) you want to display in the widget.

Filter

Select the filter you want to apply.

Period

Select the period you want to display.

Max number of bars

Enter the number of bars you want to display in the chart.

Caption

Type a caption for the widget.

Caption Link

Select to make a link to an object that is relevant to the values that are displayed in the widget.

Show Legend

Click True to display the name and color of the trend log in the widget.

Bar color

Select the color you want to use on the bars.

Y-axis minimum

Enter the Y-axis minimum.

Show period

Select to display the period as a legend.

Y-axis maximum

Enter the Y-axis maximum.

Decimals

Select the number of decimals you want to display.

  • How Dashboards Work
  • Dashboard Widgets
  • Widget Dialog Box – Layout Tab