Use the Event Pie dialog box to configure and edit an event pie.
 
    | Component | Description | 
| Column | Select the column(s) you want to display in the widget. | 
| Filter | Select the filter you want to apply. | 
| Max number of slices | Select the number of slices you want to display in the pie chart. | 
| Period | Select the period you want to display. | 
| Caption | Type a caption for the widget. | 
| Caption Link | Select to make a link to an object that is relevant to the values that are displayed in the widget. | 
| Pie Center | Select how you want to display the pie center. For more information, see Log Pie . | 
| Show Legend | Click True to display the name and color of the trend log in the widget. | 
| Show Percentage | Select to display the values in percentage. | 
| Show period | Select to display the period as a legend. | 
| Display Value | Select to display the events as legends in the slices. | 
| Decimals | Select the number of decimals you want to display. |