earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: WebStation
Функции: Dashboards
Версия продукта: 2024, 7.0
03.12.2024

Configuring an Alarm Count

You configure an alarm count to get a graphical representation of alarms.

Показать больше
action_close

An alarm count displays the number of alarms from the EcoStruxure BMS.

You can apply a filter to select the alarms based on the alarm fields.

Alarm count does not count the acknowledged alarms. Alarm count only displays the number of alarms in alarm state.

To configure an alarm count
  1. Right-click the dashboard and click Edit dashboard .

  2. Click Configure or click the Settings button

     
    action_zoom_plus_stroke
    .

  3. In the Alarm Count dialog box, click the Add filter button

     
    action_zoom_plus_stroke
    if you want to apply a filter on the alarms.

  4. In the Period box, select a period.

  5. In the Caption box, type a caption.

  6. In the Caption link box, enter a link to an object that is relevant for the alarm count.

  7. In the Show period box, select True to display the period as a legend.

  8. Click OK .

  • How Dashboards Work
  • Dashboard Widgets
  • Widget Dialog Box – Layout Tab
  • Alarm Count
  • Alarm Count Dialog Box
  • Adding a Widget to a Dashboard