earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WebStation
Funkcje: Dashboards
Wersja produktu: 2022, 2023
2024-02-23

Configuring an Event Pie

You configure an event pie chart to get a circular graphic divided into slices to illustrate proportions of events.

Pokaż więcej
action_close

An event pie chart is a circular graphic divided into slices to illustrate proportions of events.

You can select the event column you want to display. You can also apply a filter to select the event based on the event fields.

To configure an event pie
  1. Right-click the dashboard and click Edit dashboard .

  2. Click Configure or click the Settings button

     
    action_zoom_plus_stroke
    .

  3. In the Event Pie properties dialog box, in the Column box, enter the events you want to display.

  4. Click the Add filter button

     
    action_zoom_plus_stroke
    if you want to apply a filter on the alarms.

  5. In the Max number of slices box, enter the maximum number of slices you want to display in the pie.

  6. In the Calculation method box, select a calculation method.

  7. In the Caption box, type a caption.

  8. In the Caption link box, enter a link to an object that is relevant for the pie chart.

  9. In the Pie center select a pie center.

  10. In the Show Legend box, select True to display legends in the event pie.

  11. In the Show Percentage box, select True to display the values in percentage.

  12. In the Show Period box, select True to display the period as a legend.

  13. In the Display Values box, select True to display the numerical values.

  14. Click OK .

  • How Dashboards Work
  • Dashboard Widgets
  • Widget Dialog Box – Layout Tab
  • Event Pie
  • Event Pie Dialog Box
  • Adding a Widget to a Dashboard