earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WebStation
Funkcje: Dashboards
Wersja produktu: 2022, 2023
2024-02-23

Configuring an Event Rate Chart

You configure an event rate chart to get a graphical representation of event rates represented by bars.

Pokaż więcej
action_close

An event rate chart is a graphical representation of event rates represented by bars.

You can select the event column you want to display. You can also apply a filter to select the events based on the event fields.

To configure an event rate chart
  1. Right-click the dashboard and click Edit dashboard .

  2. Click Configure or click the Settings button

     
    action_zoom_plus_stroke
    .

  3. In the Event rate chart propertie s dialog box, in the Column box, select the column you want to display in the chart.

  4. Click the Add filter button

     
    action_zoom_plus_stroke
    if you want to apply a filter on the events.

  5. In the Period box, select a period.

  6. In the Caption box, type a caption.

  7. In the Caption link box, enter a link to an object that is relevant for the chart.

  8. In the Show Legend box, select True to display legends in the chart.

  9. In the Bar color field, select a color.

  10. In Y-axis minimum box, enter the minimum value of the y-axis.

  11. In the Show Period box, select True to display the period as a legend.

  12. In Y-axis maximum box, enter the maximum value of the y-axis.

  13. It the Decimals box, select the number of decimals you want to display.

  14. Click OK .

  • How Dashboards Work
  • Dashboard Widgets
  • Widget Dialog Box – Layout Tab
  • Event Rate Chart
  • Event Rate Chart Dialog Box
  • Adding a Widget to a Dashboard