earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WebStation
Funkcje: Dashboards
Wersja produktu: 2022, 2023
2024-02-23

Configuring an Event Sankey Chart

You configure an events Sankey chart to get graphically representation of events in a a Sankey chart.

Pokaż więcej
action_close

An events Sankey chart is used to graphically present a Sankey chart of the events in the EcoStruxure Building Operation system.

You can select the event column you want to display. You can also apply a filter to select the event based on the event fields.

By clicking on a flow in the chart you can view a list of event details for that particular event.

To configure an event sankey chart
  1. Right-click the dashboard and click Edit dashboard .

  2. Click Configure or click the Settings button

     
    action_zoom_plus_stroke
    .

  3. In the Alarm sankey chart dialog box, in the Colums box, enter the columns you want to display in the chart.

  4. Click the Add filter button

     
    action_zoom_plus_stroke
    if you want to apply a filter on the events.

  5. In the Period box, select a period.

  6. In the Max number of nodes box, select the number of nodes you want to display.

  7. In the Caption box, type a caption.

  8. In the Caption link box, enter a link to an object that is relevant for the chart.

  9. In the Show Legend box, select True to display the name and color of the events in the chart.

  10. In the Show period box, select True to display legends in the chart.

  11. In the Decimals box, select the number of decimals to display.

  12. Click OK .

  • How Dashboards Work
  • Dashboard Widgets
  • Widget Dialog Box – Layout Tab
  • Event Sankey Chart
  • Event Sankey Chart Dialog Box
  • Adding a Widget to a Dashboard