earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WebStation
功能: Dashboards
产品版本: 2024, 7.0
2024/12/3

Configuring an Event Sankey Chart

You configure an events Sankey chart to get graphically representation of events in a a Sankey chart.

显示更多
action_close

An events Sankey chart is used to graphically present a Sankey chart of the events in the EcoStruxure BMS.

You can select the event column you want to display. You can also apply a filter to select the event based on the event fields.

By clicking on a flow in the chart you can view a list of event details for that particular event.

To configure an event sankey chart
  1. Right-click the dashboard and click Edit dashboard .

  2. Click Configure or click the Settings button

     
    action_zoom_plus_stroke
    .

  3. In the Alarm sankey chart dialog box, in the Colums box, enter the columns you want to display in the chart.

  4. Click the Add filter button

     
    action_zoom_plus_stroke
    if you want to apply a filter on the events.

  5. In the Period box, select a period.

  6. In the Max number of nodes box, select the number of nodes you want to display.

  7. In the Caption box, type a caption.

  8. In the Caption link box, enter a link to an object that is relevant for the chart.

  9. In the Show Legend box, select True to display the name and color of the events in the chart.

  10. In the Show period box, select True to display legends in the chart.

  11. In the Decimals box, select the number of decimals to display.

  12. Click OK .

  • How Dashboards Work
  • 仪表板小部件
  • Widget Dialog Box – Layout Tab
  • Event Sankey Chart
  • Event Sankey Chart Dialog Box
  • Adding a Widget to a Dashboard