Log on to rate and give feedback
12345Log on to rate
0
Как
Продукты:
WebStation
Функции:
Базовые функции
Версия продукта:
2024, 7.0
03.12.2024
Adding a Property to the Watch Pane from the Properties Dialog Box
You can add a property to the Watch pane using the properties dialog box in WebStation.
Показать больше
action_close
You add objects to the Watch pane to monitor their live values.
For example, you can monitor the impact of a change you are about to make in your system. Property changes are immediately displayed in the Watch pane.
You can save the Watch pane with all its objects and properties so that you can use it again the next time you log on to WebStation.
To add a property to the Watch pane from the properties dialog box
In WebStation, open the properties dialog box with the property you want to add.