earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Управление пользователями
Версия продукта: 2024, 7.0
02.12.2024

Syntax for IP Address Allow List

You configure the Allow list to allow access only from specific IP addresses or from ranges of IP addresses. If nothing is configured, then all IP addresses are allowed.

You can use two different syntax for lists of IP addresses:

  • A list of line separated IP addresses:

    192.168.0.1

    127.0.0.1

  • A range of IP addresses in CIDR notation on one or many lines:

    10.0.0.0/8

    10.0.0.0/16

You can also use a combination of both.

Примечание

EcoStruxure BMS does not accept other syntax for specifying IP range, eg. 10.0.0.0 - 10.0.0.255

  • Windows Active Directory User Groups
  • User Account Group – Policies Tab
  • Creating a User Account Group