earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 用户管理
产品版本: 2024, 7.0
2024/12/2

Syntax for IP Address Allow List

You configure the Allow list to allow access only from specific IP addresses or from ranges of IP addresses. If nothing is configured, then all IP addresses are allowed.

You can use two different syntax for lists of IP addresses:

  • A list of line separated IP addresses:

    192.168.0.1

    127.0.0.1

  • A range of IP addresses in CIDR notation on one or many lines:

    10.0.0.0/8

    10.0.0.0/16

You can also use a combination of both.

注释:

EcoStruxure BMS does not accept other syntax for specifying IP range, eg. 10.0.0.0 - 10.0.0.255

  • Windows Active Directory User Groups
  • User Account Group – Policies Tab
  • Creating a User Account Group