earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: Operator Display
Funkcje: Sprzęt
Wersja produktu: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Operator Display LED

Operator Display is equipped with an LED to communicate specific messages to the user.

 
action_zoom_plus_stroke Operator Display LED
Rysunek: Operator Display LED

Tabela: LED Patterns

LED Patterns

Condition

Orange, flashing

Operator Display is starting up.

Green, constant (while running)

There are no active alarms.

Red, flashing (while running)

There is at least one active alarm that is not acknowledged.

Red, constant (while running)

There is at least one active alarm but all alarms are acknowledged.

  • Hardware Overview
  • Operator Display
  • Alarm Handling
  • Acknowledging an Alarm