earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: Operator Display
功能: 硬件
产品版本: 3.3, 2022, 2023, 2024, 7.0
2021/7/22

Installing Operator Display on a Panel

You install Operator Display on a panel in equipment rooms and small buildings to simplify operations, service, and troubleshooting.

显示更多
action_close

Operator Display is panel-mounted in equipment rooms using installation fasteners.

Operator Display is designed for use on flat surfaces of IP 65F, Type 1, Type 4X (indoor use only) and Type 13 enclosures.

Be aware of the following when building Operator Display into an end-user product:

  • The rear of Operator Display is not approved as an enclosure.

  • When building Operator Display into an end-user product, use an enclosure that satisfies standards as the end-user product’s overall enclosure.

  • Install Operator Display in an enclosure with mechanical rigidity.

  • Operator Display is not designed for outdoor use. UL certification obtained is for indoor use only.

  • Install and operate Operator Display with its front facing outward.

注释:
  • The necessary torque is 0.5 Nm (4.4 lbf.in).

  • IP 65F is not part of the UL certification.

Installation Requirements

Read the specific security hardening recommendations before installing Operator Display. 有关更多信息,请参阅 Operator Display Hardening .

小心 小心

RISK OF BURNING INJURY

Do not touch the bezel or rear chassis during operation.

Failure to follow these instructions can result in injury or equipment damage.

Before installing Operator Display, read the following list of installation requirements:

  • Check that the installation wall or cabinet surface is flat, in good condition and has no jagged edges. Metal reinforcing strips may be attached to the inside of the wall, near the panel-cut, to increase its rigidity.

  • Decide on the thickness of the enclosure wall, based on the level of strength required. Even if the installation wall thickness is within the recommended range for the panel cut dimensions, depending on wall’s material, size, and installation location of Operator Display and other devices, the installation wall could warp. To help prevent warping, the installation surface may need to be strengthened.

  • Check that the ambient air temperature and the ambient humidity are within their specified ranges in environmental specifications. When installing Operator Display in a cabinet or enclosure, the ambient air temperature is the cabinet’s or enclosure’s internal temperature. 有关更多信息,请参阅 Operator Display .

     
    action_zoom_plus_stroke

    1. Internal temperature

    2. External temperature

  • Ensure that heat from surrounding equipment does not cause this product to exceed its standard operating temperature.

  • When installing this product in a slanted position, the product front should not be inclined by more than 30 degrees.

     
    action_zoom_plus_stroke

  • For easier maintenance, operation and improved ventilation, install this product at least 100 mm (3.94 in) away from adjacent structures and other equipment as shown in the following illustration:

     
    action_zoom_plus_stroke

Pressure Differences

When applying and installing this product, it is important that steps are taken to help eliminate any pressure difference between the inside and the outside of the enclosure in which this product is mounted. Higher pressure inside the enclosure can cause delamination of the front membrane of the display. Even a small pressure difference inside the enclosure will act on the large area of the membrane and can result in sufficient force to delaminate the membrane and thus cause the failure of the touch capability. Pressure differences can often occur in applications where there are multiple fans and ventilators moving air at different rates in different rooms. Follow these techniques to help ensure that this product's function is not affected by this misapplication:

  • Seal all conduit connections inside of the enclosure, especially those that lead to other rooms that may be at a different pressure.

  • Where applicable, install a small weep hole at the bottom of the enclosure to allow equalization of the internal and external pressure.

Panel Cut Dimensions

Specific measurements must be taken into consideration when preparing to install Operator Display on a panel.

 
action_zoom_plus_stroke Panel cut dimensions
图: Panel cut dimensions

A

B

C

190 mm (+1/0 mm)

(7.48 in [+0.04/0 in])

135 mm (+1/0 mm)

(5.31 in [+0.04/0 in])

1.6 to 5 mm

(0.06 to 0.2 in)

警告 警告

HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH

  • Remove all power from the device before removing any covers or elements of the system, and prior to installing or removing any accessories, hardware, or cables.

  • Unplug the power cable from both this product and the power supply.

  • Always use a properly rated voltage sensing device to confirm power is off.

  • Replace and secure all covers or elements of the system before applying power to this product.

Failure to follow these instructions can result in death or serious injury.

通知

EQUIPMENT DAMAGE

Keep this product stabilized in the panel-cutout while you are installing or removing the screw fasteners.

Failure to follow these instructions can result in equipment damage.

To install Operator Display on a panel
  1. Place this product on a clean and level surface with the screen facing down.

  2. Check that this product’s gasket is seated securely into the bezel’s groove, which runs around the perimeter of the display frame.

    注释:

    Always use the installation gasket, since it absorbs vibration in addition to repelling water. 有关更多信息,请参阅 Replacing the Installation Gasket on Operator Display .

  3. Based on this product’s panel cut dimensions, open a mount-hole on the panel and attach this product to the panel from the front side. 有关更多信息,请参阅 Operator Display Installation .

    注释:

    This product has a hook on the top to help prevent falling during installation. Insert this product into the panel at an angle to avoid hitting the hook.

     
    action_zoom_plus_stroke

    1. Hook

  4. Insert the installation fastener hooks into the insertion slots of this product.

     
    action_zoom_plus_stroke

    1. Insertion slots

    2. Installation fastener

    3. Installation panel

  5. In a clockwise direction, tighten the installation fastener’s screws with a screwdriver. The recommended torque is 0.5 Nm (4.4 lbf.in).

     
    action_zoom_plus_stroke

    注释:

    The installation fasteners can be screwed by hand as well.

You can now make the required connections for power supply and communication with the devices it is meant to monitor.

  • Operator Display Installation
  • Removing Operator Display
  • Replacing the Installation Gasket on Operator Display
  • Replacing the Battery on Operator Display
  • Connecting Operator Display to a 24 VDC Power Supply