earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: Operator Display
Funkcje: Sprzęt
Wersja produktu: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Operator Display Regulatory and Agency Compliance and Approvals

This section provides information on regulatory and agency compliance and approvals for the SpaceLogic Operator Display.

CE - European Union (EU)

Operator Display bears the CE mark and complies with the following EU directives:

  • 2014/30/EU Electromagnetic Compatibility Directive (EMCD)

  • 2014/35/EU Low Voltage Directive (LVD)

  • 2011/65/EU Restriction of Hazardous Substances (RoHS) Directive

  • 2015/863/EU amending Annex II to Directive 2011/65/EU

Compliance with these EU directives implies conformity to harmonized European standards that are noted in the EU Declaration of Conformity. The EU Declaration of Conformity can be accessed on the Schneider Electric Exchange Extranet website, ecobuilding.schneider-electric.com

WEEE - European Union (EU)

The Operator Display and its packaging carry the waste of electrical and electronic equipment (WEEE) label, in compliance with EU directive 2012/19/EU, governing the disposal and recycling of electrical and electronic equipment in the European community.

Federal Communications Commission (FCC)

For Operator Display, the following statements apply.

This device complies with part 15 of the FCC Rules. Operation is subject to the following two conditions:

  • This device may not cause harmful interference.

  • This device must accept any interference received, including interference that may cause undesired operation.

This equipment has been tested and found to comply with the limits for a Class A digital device, pursuant to part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference when the equipment is operated in a commercial environment. This equipment generates, uses, and can radiate radio frequency energy and, if not installed and used in accordance with the instruction manual, may cause harmful interference to radio communications. Operation of this equipment in a residential area is likely to cause harmful interference in which case the user will be required to correct the interference at his own expense.

Properly shielded and grounded cables and connectors must be used in order to meet FCC emission limits. Schneider Electric is not responsible for any radio or television interference caused by using other than recommended cables and connectors or by unauthorized changes or modifications to this equipment. Unauthorized changes or modifications could void the user's authority to operate the equipment.

Innovation, Science and Economic Development Canada (ISED)

For Operator Display, the following statements apply.

This digital apparatus does not exceed the Class A limits for radio noise emissions from digital apparatus as set out in the Radio Interference Regulations of the Canadian Department of Communications.

Cet appareil numérique ne dépasse pas les limites de la Classe A pour les émissions radio bruit des appareils numériques, tel qu'énoncé dans le Règlement sur le brouillage radioélectrique du ministère des Communications du Canada.

Canada ICES-003 (A) / NMB-003 (A)

UL

Operator Display is a UL Listed product for the United States and Canada.

Operator Display complies with the following UL standards:

  • UL CSA 22.2 61010-1

  • UL CSA 22.2 61010-2-201

Any changes or modifications to the product may invalidate the certificate.

UK Conformity Assessed

S.I. 2016/1091 - Electromagnetic Compatibility Regulations 2016

S.I. 2016/1101 - Electrical Equipment (Safety) Regulations 2016

S.I. 2012/3032 - Restriction of the Use of Certain Hazardous Substances in Electrical and Electronic Equipment Regulations 2012

This equipment complies with the rules, of the UK regulations, for governing the UKCA Marking for the United Kingdom specified in the above directive(s).

  • Hardware Overview
  • Operator Display