earth_america
user_standard Anmelden
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Konzept

Konzept


Produkte: Operator Display
Funktionen: Hardware
Produktversion: 3.3, 2022, 2023, 2024, 7.0
22.07.2021

Operator Display Safety Information

This section provides safety information specific to Operator Display. Carefully read the instructions before trying to install, operate, service, or maintain the equipment.

The Operator Display specific safety instructions below are used with the standard safety information. Für weitere Informationen siehe Sicherheitsinformationen .

Never open the equipment. For safety reasons, the equipment should be opened only by qualified service personnel. If one of the following situations arises, get the equipment checked by service personnel:

  • The power cord or plug is damaged.

  • Liquid has penetrated into the equipment.

  • The equipment has been exposed to moisture.

  • The equipment does not work well, or you cannot get it to work according to the user documentation.

  • The equipment has been dropped and damaged.

  • The equipment has obvious signs of breakage.

Hinweis

Opening the equipment to make any changes or modifications to the equipment may invalidate all applicable regulatory and agency certifications and approvals.

Hinweis

EQUIPMENT DAMAGE

  • Do not leave this equipment in an environment where the storage temperature may go below -20 °C (-4 °F) or above 60 °C (140 °F).

  • Ensure this product is not in permanent and direct contact with oils.

  • Do not press on the display of this product with excessive force or with a hard object.

  • Do not press on the touch screen with a pointed object, such as the tip of a mechanical pencil or a screwdriver.

Failure to follow these instructions can result in equipment damage.

Operator Display contains a battery that provides power to the internal real-time clock (RTC). There is a risk of explosion if the battery is incorrectly replaced.

Operator Display contient une pile qui alimente l’horloge en temps réel interne. Il y a un risque d’explosion si la pile est remplacée incorrectement.

Warnung Warnung

HAZARD OF EXPLOSION OR EQUIPMENT DAMAGE

  • Replace the battery only with same or equivalent battery type recommended by the manufacturer.

  • Discard used batteries according to the manufacturer's instructions.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

 
action_zoom_plus_stroke

  • Hardware Overview
  • Operator Display
  • Operator Display Installation
  • Sicherheitsinformationen