earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: WebStation
Функции: Расписания
Версия продукта: 2024, 7.0
02.12.2024

Multi Schedule Viewer Toolbar

Use the Multi Schedule Viewer toolbar to select, add and remove schedules.

Таблица: Multi Schedule Viewer Toolbar

Button

Description

 
action_zoom_plus_stroke

Add schedules

Click to add a schedule to the Multi schedule viewer.

 
action_zoom_plus_stroke

Remove selected schedules

Click to remove the selected schedule from the Multi schedule viewer.

Go to date

Click to open the calendar to go to a specific date.

 
action_zoom_plus_stroke

Select all

Click to select all schedules in the Multi schedule viewer.

 
action_zoom_plus_stroke

Deselect all

Click to deselect all schedules in the Multi schedule viewer.

 
action_zoom_plus_stroke

Drag exception event/Drag weekly event

Click to change between adding exception events and weekly events.

 
action_zoom_plus_stroke

Settings

Click to open the Multi schedule value toolbar .

Assign on click

Click to assign a value on click so that you can give an event a value with one click.

  • Multi Schedule Viewer
  • Multi Schedule Viewer Workspace