The RP-V controller is available in two models that support both BACnet/IP and MS/TP communication. These two models offer two different combinations (sets) of the number of I/O points and types of I/O points. The RP-V controller also comes in a model that only supports BACnet MS/TP communication.
Range |
Model |
BACnet |
I/O Set |
I/O Points |
SpaceLogic RP-V Advanced |
RP-V-4A |
IP or MS/TP a |
4A |
4 |
SpaceLogic RP-V Advanced |
RP-V-5A |
IP or MS/TP a |
5A |
5 |
EasyLogic RP-V |
RP-V-5C-M |
MS/TP |
5C |
5 |
Более подробную информацию см. RP-V Onboard I/O .
The RP-V controllers have the same compact design and approximately the same dimensions as the MP-V controllers and a majority of the Schneider Electric VAV controller models from Andover Continuum, TAC Vista, and TAC I/A Series product lines. You can use the RP-V controllers for both cooling and heating applications.
The EasyLogic RP-V model differs significantly from the SpaceLogic RP-V models not only in terms of the supported BACnet communication protocol(s), but also with regards to the set of communication ports and several other features.
The EasyLogic models have an “-M” in the product name.
Feature |
RP-V-4A, RP-V-5A |
RP-V-5C-M |
Built-in wireless connectivity |
yes |
no a |
Ethernet ports |
2 |
0 |
USB ports |
1 b |
0 |
RS-485 ports with RJ45 interface |
2 (Com A, Com B) c |
1 (Com A) d |
RS-485 ports supporting Isolated RS-485 Adapter e |
Com B |
- |
RS-485 ports supporting Non-isolated RS-485 Adapter or RS-485 Power Adapter f |
Com A, Com B |
Com A |
RS-485 port with screw terminals |
0 |
1 g |
I/O and power input terminals/connectors |
Fixed screw terminals |
Fixed screw terminals |
MS/TP address configuration |
Software |
DIP switch |
Room bus support |
yes |
no |
Sensor bus support |
yes |
yes h |
Modbus support |
yes i |
yes h j |
RTD sensor support |
yes |
no |
LED(s) |
1 k |
1 k |
Real-time clock |
yes |
no |
Input power |
24 VAC |
24 VAC |
Power input type |
Isolated |
Isolated |
CPU type |
Single-core |
Single-core |
Memory (RAM / NOR flash / FRAM) |
6 MB / 48 MB / 128 kB |
6 MB / 32 MB / 128 kB l |