earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: RP-V
功能: 硬件
产品版本: 2022, 2023, 2024, 7.0
2023/3/30

RP-V Screw Terminals

arrow1_rotationRP-V-4A Screw Terminals arrow1_rotationRP-V-5A Screw Terminals arrow1_rotationRP-V-5C-M Screw Terminals

The RP-V has fixed screw terminals for the power input, SSR outputs, and universal inputs/outputs. The RP-V-5C-M model also has a removable screw terminal block for connection to the BACnet MS/TP (RS-485) network.

The wiring recommendations are provided separately. 有关更多信息,请参阅 Wiring .

RP-V-4A Screw Terminals

The RP-V-4A model has four I/O points and the controller is equipped with 11 fixed screw terminals.

有关更多信息,请参阅 RP-V-4A Screw Terminals .

RP-V-5A Screw Terminals

The RP-V-5A model has five I/O points and the controller is equipped with 11 fixed screw terminals.

有关更多信息,请参阅 RP-V-5A Screw Terminals .

RP-V-5C-M Screw Terminals

The RP-V-5C-M model has five I/O points and the controller is equipped with 11 fixed screw terminals and a 3-position removable screw terminal block.

有关更多信息,请参阅 RP-V-5C-M Screw Terminals .

  • RP-V Controllers
  • RP-V Models
  • RP-V-4A Screw Terminals
  • RP-V-5A Screw Terminals
  • RP-V-5C-M Screw Terminals
  • Wiring