Produkty: Operator Display
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Values/Multi-State Detail Screen

Use the Values/Multi-State detail screen to display and edit the seleted multi-state value.

Ostrzeżenie Ostrzeżenie

Unintended equipment operation

Do not force values without knowing the effect.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

 
action_zoom_plus_stroke Values/Multi-State detail screen
Rysunek: Values/Multi-State detail screen

Tabela: Values/Multi-State Detail Screen

Component

Description

Force

Tap Force to override the value received from the device. Więcej informacji zawiera Value Editing .

Value

Tap a value option. The value options differ depending on what the multi-state value is used for in the system.

  • Value Editing