earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: Operator Display
Funktionaliteter: Grundläggande funktionalitet
Produktversion: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Values/Multi-State Detail Screen

Use the Values/Multi-State detail screen to display and edit the seleted multi-state value.

Varning Varning

Unintended equipment operation

Do not force values without knowing the effect.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

 
action_zoom_plus_stroke Values/Multi-State detail screen
Figur: Values/Multi-State detail screen

Tabell: Values/Multi-State Detail Screen

Component

Description

Force

Tap Force to override the value received from the device. Mer information finns i Value Editing .

Value

Tap a value option. The value options differ depending on what the multi-state value is used for in the system.

  • Value Editing